Part Number: THVD8000
Other Parts Discussed in Thread: THVD8010
The contents below are about performing OOK operation at -40℃, and we request technical support for the operation.
The two waveforms below are measured from one communication packet.
![]() |
![]() |
|
1. Abnormal waveform |
2. Normal waveform |
Waveform description
Yellow: Master Rx, Green: Master A-B, Red: Slave Tx, Blue: Slave A-B
The support request is to error operation and normal operation in the part of the oscillating (58 kHz and 104kHz) after the ON/OFF keying (500 kHz).
- Request technical support for the reason for error operation at 58 kHz.
- Request technical support for the reason for normal operation at 104 kHz.