Part Number: DS90UB954-Q1
Hi,
I am working on a project involving the couple deserialize DS90UB954 and serializer DS90UB953.
We are working on two different strategies at the same time to discover which is the best one for our application: on one hand we developed a board based on coaxial connection and we had some layout problems we are trying to solve thanks to your suggestion (DS90UB954-Q1: Communication issue - Margin Analysis show low margin - Interface forum - Interface - TI E2E support forums); on the other hand, we are trying a solution based on STP connection.
We found few matherial on datasheet about STP, so I have a few questions:
- concerning layout the only difference between stp and coaxial is that there are differential traces with 100 Ohm impedance, instead of a single-ended line with 50Ohm impedance. Is it correct? All the suggestions you gave me here DS90UB954-Q1: Communication issue - Margin Analysis show low margin - Interface forum - Interface - TI E2E support forums are still valid?
- we decided to use a standard Ethernet cable (4 wire pairs) to connect deserializer and serializer. In particular we want to use a differential pair to carry the signal and the remaining 3 pairs to carry power. in this way we can avoid any PoC-like filter. Do you think it is a good practice or do you expect any problem?
- Different categories of Ethernet cables exist with different shielding layout and different bandwidth. We already developed our custom ser and deser board with ethernet connector and we already tested the differences between a category 5 cable and a category 6 wire: the Margina Analysis test clearly shows a big improvement using the category 6 cable, but unfortunately the margin is still low. Do you have exxperience with standard ethernet cables to connect ser and deser? Which is the minimum required bandwidth and shilding? In other words, which cable category do you suggest to guarantee a proper transmission?
Thank you in advance.
Best regards,
Alessandro