Part Number: TUSB8042A
ESD devices had little impact.
Is there anything else that you have noticed?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We are looking into this and will get back to you shortly.
Thanks,
Zach
This matter is a continuation of the email I had with BRIAN until 4/15/2023.
[TUSB8042A USB3.0 Compatibility Test Upstream Fail]
sorry, just find out it's old issue which failed RX short channel JTOL. , how long is trace of TX/RX for upstream port ?
Best
Brian
I previously sent you a schematic and a PCB artwork drawing. On April 12, 2023, we received the following response.
”Trace for upstream port looks fine, only 2 in or 1db loss at 5Gbps.”
t looks weird it can pass RX long channel but failed short channel, Can customer send system to Dallas for test.
Best
brian
The following results are from upstream
RX:Long is Pass, Short is Fail.
TX: long is Fail, short is pass.
The test report is attached again.USB-IF_Hub_RX_USB3.2_SS_Fail_02212023_Legacy.pdfUSB-IF_Hub_UFP_TD1p3_USB3.2_SS_Fail_02212023_Legacy.pdf
for RX test, did they have a good equipment calibration? it should not fail at lo freence.
Best
Brian
The test was conducted at the test site, so the calibration is determined to be performed as a routine.
We apologize. The product is in the development stage and cannot be shipped for testing.
If there is nothing else we are aware of regarding this matter, we will close it for now.
Thank you