Other Parts Discussed in Thread: THVD1450, THVD1550
This part SN65HVD09 is provided with thermal shutdown feature. Please confirm whether its provided with short circuit protection, In case if transceiver used as RS422 driver / Tx ouput gets shorted whether it will limit the current or enter into standby mode or high impedance state without causing any damage to the device.
If not supported pls suggest the TI part with the short circuit protection and having Tx/ Rx RS422 section upto 9 Channels