This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD3088E: Pin Assign of SN65HVD3088ENSR

Part Number: SN65HVD3088E

Dear Specialists,

My customer is considering SN65HVD3088ENSR and has a question.

I would be grateful if you could advise.

---

According to the datasheet P.5 Fugure5-2, it is drawn pin assign.

However, A, B, Z, and Y pin assignments are shown, and it is Full Duplex.

...

For Half Duplex, I think only A and B are pin assigned.

Could you please let me know the exact pin assignment.

For example,

A(12) and B(11) are NC

Z(10) and Y(9) are NC

others

---

I appreciate your great help and cooperation.

Best regards,

Shinichi

  • Shinichi,

    There is currently a misprint for the NSR package - we have a datasheet update being approved right now.

    Pins 11 and 12 (A and B as listed now) are not electrically connected.

    Pins 9 and 10 (Y and Z) act as a standard Half-duplex device (so input and output). It is not full-duplex; there was a miscommunication published in the first NSR package update.

    Best,

    Parker Dodson

     

  • Hi Parker,

    Thank you for your reply.

    I understand.

    SN65HVD3088NSR is half duplex, 9pin(Y) and 10pin(Z) act as input and output.

    I'll share this information with the customer.

    I appreciate your great help and cooperation.

    Best regards,

    Shinichi