This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867E: Polarity detection and correction

Part Number: DP83867E


Hi team,

According to this thread, polarity detection and correction feature is supported at DP83867.

  1. When reverse polarity is detected on DP83867's RX side, does its TX side flip output polarity accordingly as there is possibility that TX side is also reversed?
    Or detection result of polarity on RX side doesn't affect to TX side?
  2. Polarity detection and correction seems required by IEEE802.3. Does all Ethernet PHY have this feature?

Best regards,

Shota Mago

  • Hello,

    The PHY will detect and correct polarity as needed per each channel. 

    Yes, all PHYs that conform to IEEE802.3 should have this.

    Sincerely,

    Gerome

  • Hi Gerome,

    Thanks for your reply. Let me clarify your answer.

    The PHY will detect and correct polarity as needed per each channel. 

    Does this mean TX side of DP83867E also have polarity correction? Although this is Microchip's app note, it states "For 10BASE-T links the IEEE 802.3 requires the Ethernet PHY to support autopolarity detection and correction of the received data.". So it seems that polarity detection/correction feature is supported by Rx side.

    Also, what I'd like to confirm is that when Rx side detects reverse polarity, if the device automatically flip polarity of Tx side or not.

    Best regards,

    Shota Mago

  • Hello Shota,

    What speed is the customer looking to use? In 1G, there is no explicit TX and RX on MDI. 

    Is customer seeing an issue where the polarity is being swapped on TX due to RX?

    Sincerely,

    Gerome

  • Hi Gerome,

    The customer accepted answer of "all PHYs that conform to IEEE802.3 should have this.".

    So you can close the thread. Thank you so much for your support.

    Best regards,

    Shota Mago