Part Number: AM26LS32AC
Other Parts Discussed in Thread: SN65LBC173A, AM26LV32, SN75LBC173A
I am using an AM26LS32ACPWR. There is a 100-ohm termination resistor between the A and B inputs. When these inputs are floating, I expect to see a high on the Y output due to the fail-safe function in this device. However, on some of the boards, the Y output is low. Is there something I can do besides adding pullup/pulldown resistors on the A and B inputs?