Part Number: DP83867E
We are presently in the process of initializing DP83867E Ethernet interface(SGMII). However, we are encountering difficulties in establishing a connection to the network despite utilizing the provided drivers (this driver looks like RGMII driver, we need SGMII drivers) and configuring the strap options as specified in the attached schematics. We kindly request your assistance and guidance in identifying any necessary modificationreadme.docxs to ensure its proper functionality.Ethernet PHY.pdf
/*
* Driver for the Texas Instruments DP83867 PHY
*
* Copyright (C) 2015 Texas Instruments Inc.
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License as published by
* the Free Software Foundation; either version 2 of the License.
*
* This program is distributed in the hope that it will be useful,
* but WITHOUT ANY WARRANTY; without even the implied warranty of
* MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include <linux/ethtool.h>
#include <linux/kernel.h>
#include <linux/mii.h>
#include <linux/module.h>
#include <linux/of.h>
#include <linux/phy.h>
#include <dt-bindings/net/ti-dp83867.h>
#define DP83867_PHY_ID 0x2000a231
#define DP83867_DEVADDR 0x1f
#define MII_DP83867_PHYCTRL 0x10
#define MII_DP83867_MICR 0x12
#define MII_DP83867_ISR 0x13
#define DP83867_CTRL 0x1f
#define DP83867_CFG3 0x1e
/* Extended Registers */
#define DP83867_CFG4 0x0031
#define DP83867_RGMIICTL 0x0032
#define DP83867_STRAP_STS1 0x006E
#define DP83867_RGMIIDCTL 0x0086
#define DP83867_IO_MUX_CFG 0x0170
#define DP83867_SW_RESET BIT(15)
#define DP83867_SW_RESTART BIT(14)
/* MICR Interrupt bits */
#define MII_DP83867_MICR_AN_ERR_INT_EN BIT(15)
#define MII_DP83867_MICR_SPEED_CHNG_INT_EN BIT(14)
#define MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN BIT(13)
#define MII_DP83867_MICR_PAGE_RXD_INT_EN BIT(12)
#define MII_DP83867_MICR_AUTONEG_COMP_INT_EN BIT(11)
#define MII_DP83867_MICR_LINK_STS_CHNG_INT_EN BIT(10)
#define MII_DP83867_MICR_FALSE_CARRIER_INT_EN BIT(8)
#define MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN BIT(4)
#define MII_DP83867_MICR_WOL_INT_EN BIT(3)
#define MII_DP83867_MICR_XGMII_ERR_INT_EN BIT(2)
#define MII_DP83867_MICR_POL_CHNG_INT_EN BIT(1)
#define MII_DP83867_MICR_JABBER_INT_EN BIT(0)
/* RGMIICTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_EN BIT(1)
#define DP83867_RGMII_RX_CLK_DELAY_EN BIT(0)
/* STRAP_STS1 bits */
#define DP83867_STRAP_STS1_RESERVED BIT(11)
/* PHY CTRL bits */
#define DP83867_PHYCR_FIFO_DEPTH_SHIFT 14
#define DP83867_PHYCR_FIFO_DEPTH_MASK (3 << 14)
#define DP83867_PHYCR_RESERVED_MASK BIT(11)
/* RGMIIDCTL bits */
#define DP83867_RGMII_TX_CLK_DELAY_SHIFT 4
/* IO_MUX_CFG bits */
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL 0x1f
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX 0x0
#define DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN 0x1f
/* CFG4 bits */
#define DP83867_CFG4_PORT_MIRROR_EN BIT(0)
enum {
DP83867_PORT_MIRROING_KEEP,
DP83867_PORT_MIRROING_EN,
DP83867_PORT_MIRROING_DIS,
};
struct dp83867_private {
int rx_id_delay;
int tx_id_delay;
int fifo_depth;
int io_impedance;
int port_mirroring;
bool rxctrl_strap_quirk;
};
static int dp83867_ack_interrupt(struct phy_device *phydev)
{
int err = phy_read(phydev, MII_DP83867_ISR);
if (err < 0)
return err;
return 0;
}
static int dp83867_config_intr(struct phy_device *phydev)
{
int micr_status;
if (phydev->interrupts == PHY_INTERRUPT_ENABLED) {
micr_status = phy_read(phydev, MII_DP83867_MICR);
if (micr_status < 0)
return micr_status;
micr_status |=
(MII_DP83867_MICR_AN_ERR_INT_EN |
MII_DP83867_MICR_SPEED_CHNG_INT_EN |
MII_DP83867_MICR_AUTONEG_COMP_INT_EN |
MII_DP83867_MICR_LINK_STS_CHNG_INT_EN |
MII_DP83867_MICR_DUP_MODE_CHNG_INT_EN |
MII_DP83867_MICR_SLEEP_MODE_CHNG_INT_EN);
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
micr_status = 0x0;
return phy_write(phydev, MII_DP83867_MICR, micr_status);
}
static int dp83867_config_port_mirroring(struct phy_device *phydev)
{
struct dp83867_private *dp83867 =
(struct dp83867_private *)phydev->priv;
u16 val;
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);
if (dp83867->port_mirroring == DP83867_PORT_MIRROING_EN)
val |= DP83867_CFG4_PORT_MIRROR_EN;
else
val &= ~DP83867_CFG4_PORT_MIRROR_EN;
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);
return 0;
}
#ifdef CONFIG_OF_MDIO
static int dp83867_of_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867 = phydev->priv;
struct device *dev = &phydev->mdio.dev;
struct device_node *of_node = dev->of_node;
int ret;
if (!of_node)
return -ENODEV;
dp83867->io_impedance = -EINVAL;
/* Optional configuration */
if (of_property_read_bool(of_node, "ti,max-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MAX;
else if (of_property_read_bool(of_node, "ti,min-output-impedance"))
dp83867->io_impedance = DP83867_IO_MUX_CFG_IO_IMPEDANCE_MIN;
dp83867->rxctrl_strap_quirk = of_property_read_bool(of_node,
"ti,dp83867-rxctrl-strap-quirk");
ret = of_property_read_u32(of_node, "ti,rx-internal-delay",
&dp83867->rx_id_delay);
if (ret &&
(phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID))
return ret;
ret = of_property_read_u32(of_node, "ti,tx-internal-delay",
&dp83867->tx_id_delay);
if (ret &&
(phydev->interface == PHY_INTERFACE_MODE_RGMII_ID ||
phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID))
return ret;
if (of_property_read_bool(of_node, "enet-phy-lane-swap"))
dp83867->port_mirroring = DP83867_PORT_MIRROING_EN;
if (of_property_read_bool(of_node, "enet-phy-lane-no-swap"))
dp83867->port_mirroring = DP83867_PORT_MIRROING_DIS;
return of_property_read_u32(of_node, "ti,fifo-depth",
&dp83867->fifo_depth);
}
#else
static int dp83867_of_init(struct phy_device *phydev)
{
return 0;
}
#endif /* CONFIG_OF_MDIO */
static int dp83867_config_init(struct phy_device *phydev)
{
struct dp83867_private *dp83867;
int ret, val, bs;
u16 delay;
if (!phydev->priv) {
dp83867 = devm_kzalloc(&phydev->dev, sizeof(*dp83867),
//dp83867 = devm_kzalloc(&phydev->mdio.dev, sizeof(*dp83867),
GFP_KERNEL);
if (!dp83867)
return -ENOMEM;
phydev->priv = dp83867;
ret = dp83867_of_init(phydev);
if (ret)
return ret;
} else {
dp83867 = (struct dp83867_private *)phydev->priv;
}
/* RX_DV/RX_CTRL strapped in mode 1 or mode 2 workaround */
if (dp83867->rxctrl_strap_quirk) {
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4);
val &= ~BIT(7);
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_CFG4, val);
}
printk("********** %s %d\n",__func__,__LINE__);
#if 0
if (phy_interface_is_rgmii(phydev)) {
val = phy_read(phydev, MII_DP83867_PHYCTRL);
if (val < 0)
return val;
val &= ~DP83867_PHYCR_FIFO_DEPTH_MASK;
val |= (dp83867->fifo_depth << DP83867_PHYCR_FIFO_DEPTH_SHIFT);
/* The code below checks if "port mirroring" N/A MODE4 has been
* enabled during power on bootstrap.
*
* Such N/A mode enabled by mistake can put PHY IC in some
* internal testing mode and disable RGMII transmission.
*
* In this particular case one needs to check STRAP_STS1
* register's bit 11 (marked as RESERVED).
*/
bs = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_STRAP_STS1);
if (bs & DP83867_STRAP_STS1_RESERVED)
val &= ~DP83867_PHYCR_RESERVED_MASK;
ret = phy_write(phydev, MII_DP83867_PHYCTRL, val);
if (ret)
return ret;
/* Set up RGMII delays */
val = phy_read_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_ID)
val |= (DP83867_RGMII_TX_CLK_DELAY_EN | DP83867_RGMII_RX_CLK_DELAY_EN);
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_TXID)
val |= DP83867_RGMII_TX_CLK_DELAY_EN;
if (phydev->interface == PHY_INTERFACE_MODE_RGMII_RXID)
val |= DP83867_RGMII_RX_CLK_DELAY_EN;
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIICTL, val);
delay = (dp83867->rx_id_delay |
(dp83867->tx_id_delay << DP83867_RGMII_TX_CLK_DELAY_SHIFT));
phy_write_mmd(phydev, DP83867_DEVADDR, DP83867_RGMIIDCTL,
delay);
if (dp83867->io_impedance >= 0) {
val = phy_read_mmd(phydev, DP83867_DEVADDR,
DP83867_IO_MUX_CFG);
val &= ~DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
val |= dp83867->io_impedance &
DP83867_IO_MUX_CFG_IO_IMPEDANCE_CTRL;
phy_write_mmd(phydev, DP83867_DEVADDR,
DP83867_IO_MUX_CFG, val);
}
}
#endif
/* Enable Interrupt output INT_OE in CFG3 register */
if (phy_interrupt_is_valid(phydev)) {
val = phy_read(phydev, DP83867_CFG3);
val |= BIT(7);
phy_write(phydev, DP83867_CFG3, val);
}
if (dp83867->port_mirroring != DP83867_PORT_MIRROING_KEEP)
dp83867_config_port_mirroring(phydev);
return 0;
}
static int dp83867_phy_reset(struct phy_device *phydev)
{
int err;
err = phy_write(phydev, DP83867_CTRL, DP83867_SW_RESET);
if (err < 0)
return err;
return dp83867_config_init(phydev);
}
static struct phy_driver dp83867_driver[] = {
{
.phy_id = DP83867_PHY_ID,
.phy_id_mask = 0xfffffff0,
.name = "TI DP83867",
.features = PHY_GBIT_FEATURES,
.flags = PHY_HAS_INTERRUPT,
.config_init = dp83867_config_init,
.soft_reset = dp83867_phy_reset,
/* IRQ related */
.ack_interrupt = dp83867_ack_interrupt,
.config_intr = dp83867_config_intr,
.config_aneg = genphy_config_aneg,
.read_status = genphy_read_status,
.suspend = genphy_suspend,
.resume = genphy_resume,
},
};
//module_phy_driver(dp83867_driver);
static int __init dp83867_init(void)
{
return phy_driver_register(&dp83867_driver);
}
static void __exit dp83867_exit(void)
{
// dp83640_free_clocks();
phy_driver_unregister(&dp83867_driver);
}
module_init(dp83867_init);
module_exit(dp83867_exit);
static struct mdio_device_id __maybe_unused dp83867_tbl[] = {
{ DP83867_PHY_ID, 0xfffffff0 },
{ }
};
MODULE_DEVICE_TABLE(mdio, dp83867_tbl);
MODULE_DESCRIPTION("Texas Instruments DP83867 PHY driver");
MODULE_AUTHOR("Dan Murphy <dmurphy@ti.com");
MODULE_LICENSE("GPL");

Below are the observation after update.