Part Number: DP83TD510E
I am having problems using DP83TD510E.
Environment:
DP83TD510E works in rmii slave mode. Soc provides a 50Mhz clock to the xi pod.
CRS_DV/RX_DV Pin 18 is configured as CRS_DV (default).
Receiver with tapping at 50 Ω (Recommended).
The id of the phy chip is set to 0.
linux system from the following github link.
https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/net/phy/dp83td510.c
&fec1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet1>;
phy-mode = "rmii";
phy-handle = <ðphy0>;
phy-reset-gpios = <&gpio1 1 GPIO_ACTIVE_LOW>;
phy-reset-duration = <2>;
status = "okay";
};
&fec2 {
......
mdio {
#address-cells = <1>;
#size-cells = <0>;
ethphy0: ethernet-phy@0 {
compatible = "ethernet-phy-id2000.0180";
reg = <0>;
clocks = <&clks IMX6UL_CLK_ENET_REF>;
clock-names = "rmii-ref";
};
......
};
};
......
pinctrl_enet1: enet1grp {
fsl,pins = <
MX6UL_PAD_ENET1_RX_EN__ENET1_RX_EN 0x1b0b0
MX6UL_PAD_ENET1_RX_ER__ENET1_RX_ER 0x1b0b0
MX6UL_PAD_ENET1_RX_DATA0__ENET1_RDATA00 0x1b0b0
MX6UL_PAD_ENET1_RX_DATA1__ENET1_RDATA01 0x1b0b0
MX6UL_PAD_ENET1_TX_EN__ENET1_TX_EN 0x1b0b0
MX6UL_PAD_ENET1_TX_DATA0__ENET1_TDATA00 0x1b0b0
MX6UL_PAD_ENET1_TX_DATA1__ENET1_TDATA01 0x1b0b0
MX6UL_PAD_ENET1_TX_CLK__ENET1_REF_CLK1 0x4001b039
MX6UL_PAD_GPIO1_IO01__GPIO1_IO01 0xb0
>;
};
......
The DP83TD510E is always in the Link is down state, and I don't know how to deal with it. The DP83TD510E has been registered.
I tried to test Loopback Modes, but I still don't know how to handle it.