Part Number: ESD751
Dear Experts,
Are the ESD diodes are to be connected across the line and signal return or the earth(chasis)?
Regards,
Rajesh BN.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ESD751
Dear Experts,
Are the ESD diodes are to be connected across the line and signal return or the earth(chasis)?
Regards,
Rajesh BN.
Hi Rajesh,
If I am interpreting your question correctly, you are asking whether the protection diode is connected in series or in parallel. Please correct me if I am wrong, but I have provided a few images that should be helpful.

The image below shows the ESD diode should be connected in parallel with the protected IC/device.

I am not sure if you were specifically asking about ESD751 but hopefully the above application diagram helps explain where this device fits into the system.
Please let me know if you have additional questions.
Best Regards,
McKenzie Eaker
Dear Eaker,
I am afraid your interpretation is not I meant. Anyways, the diagram you have attached helps to put the question more clearly. The circuit shows the ESD diodes are connected across the line and signal return.
My doubt is, do the ESD diodes are connected between line and earth(i.e chassis).
Regards,
Rajesh BN.
Hi Rajesh,
My apologies for interpreting your question wrong. Yes, for ESD diodes it is best to connect the ground pin to the ground chassis. This shunts current away from the sensitive device in your application. Please refer to the following E2E posts for more clarification: link1, link2
Please let me know if you have additional questions or comments.
Best Regards,
McKenzie