Part Number: DS320PR1601
Hi,
1.in DS320PR1601 datasheet (page23) it is specified that Rx detection happens either by manually triggering via PD pins or via writing to respective I2C register .
Also in DS320PR1601 EVM user manual it is specified that all PD pins for all channels has to be GND to enable all channels and for x16 lane application. Will it differ if the output side is 4x4 ports?
How this pin is manually triggered?
is the respective I2C register is PD override register or Rx detect control register?
could you please tell how the above two registers has to be used?
2.Are the registers General register,Device ID0 register, Device ID1 register, common for all channels?
if so then to read above registers do we need send to particular channel address, can't we read the whole retimer using a single slave address?
3.
In the programming guide table 2-4, channel register base address is specified, but there up to channel 7 is specified. How can we access other channels upto 15.
Also by broadcast write channel bank 0 and 1(0x80), will 16 channels on A and B side be written?
How to decide the CTLE index value?
In programming guide, table 4-1, flat gain of 0dB is specified for multiple CTLE index values(0,1,2,5,6,7,8,9,10,11,12,13,14,15,16,17,18).It is mentioned in the EVM user manual and DS320PR1601 datasheet flat gain of 0dB is better and the default value.
Thanks and Regards,
Shekha Shoukath