Part Number: TUSB2036
What is the correct way to wire the connection to use for a usb c 3.0 connection.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB2036
What is the correct way to wire the connection to use for a usb c 3.0 connection.
Hi,
Please see this e2e thread on the possible USB2 connection, https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1254983/tusb2036-developing-usb-solution-tablet-host-charging-usbc-pd-input. Do you want to provide power over USB-C as well?
Thanks
David
Yes, I also want to provide power over usbc. Do you have any options? Currently using the mp5031.
Hi,
Is the tablet going to be a USB data source and sink, and power source and sink? For downstream, I draw a rough block diagram as shown below,

The MP5031 will provide Type-C charging function, while the hub provides USB2 SDP function without the BC1.2. If you need BC1.2, then you can use our USB2 or USB3 hub which support BC1.2.
You will also need to make sure the MP5031 disables its BC1.2 and configure one of its GPIO as OVERCURRENT pin and feeds back to the hub.
Thanks
David


We are currently testing the hub by itself but are having issues connecting with over usb c, it does not appear to the system. The design works as intended with USB A. This is a schematic of the usb c port.
Hi,
So if the TUSB2036 upstream port is connected to a USB host with a Type-A connector, it is able to be recognized.
But if TUSB2036 is connected to a host with USB-C connector, it is not able to be recognized, is my understanding correct?
In this case, can you check the VBUS voltage when connected to a USB-C connector, are you seeing 5V?
Can you also share the TUSB2036 hub schematic?
Thanks
David
Hi,
No, I want to make sure the source is able to provide the 5V on VBUS. With 5V on VBUS, and if you check TUSB2036 DP0 (pin 1), are you seeing it being pulled to 3.3V? This would indicate to the source that TUSB2036 is being connected.
Thanks
David