Part Number: DS110DF410
Are there any issues that can occur with 3 retimer devices back-to-back-to-back (i.e. placed very close to each other in series)? Background: For manufacturing test of our production module, we’ve designed a test board/fixture that has a retimer to help ensure that the signal amplitude going into the module is sufficient during a loopback test. On the production module (i.e. Unit Under Test), there will be a retimer on the output, and another retimer on its input. Both of these retimers are within a couple of inches of the connector that goes to the test board. Therefore, the retimer on the test board will be receiving a signal that gets retimed/boosted on the output of the UUT, and will send the retimed/boosted signals (2nd retimer) into another retimer (3rd retimer) on the UUT. As mentioned before, there is only a couple of inches of circuit board trace and a connector between each retimer.