Part Number: DS90UB935-Q1
Dears,
Customer use the DS90UB935 with DVR Project,now they want to konw the Register configuration,can you help to provide the Register configuration.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB935-Q1
Dears,
Customer use the DS90UB935 with DVR Project,now they want to konw the Register configuration,can you help to provide the Register configuration.
Thanks
Ning,
Can we get more information here? What Des are you going to connect to? What do you need to program on the 935?
Glenn
Hi Ning,
Following up here, the configuration necessary on the UB935 will differ based on the use case which you have designed here.
For example, there are features such as clk_out, frame sync, and gpio pass through which will vary in each system. Details on how to configure these different features are included in the UB935 datasheet in section 7 (detailed feature descriptions are located here). Please let me know if there's any features which you have questions on the implementation.
Best,
Thomas
Hi Ning,
The register configuration here will depend on the use case desired. If there are questions which you have on specific features of the UB935 please let me know.
Best,
Thomas
Hi Thomas,
Now I wait customer's feedback,once I got it will let you know.
Thanks
Thanks Ning, please let me know when you hear update back from customer.