Part Number: TCAN1042HV
Hi Team,
My customer is using TCAN1042, and now they observe that the voltage level of ACK bit is much higher than other bits, as the waveform shown below.
As I learned from another e2e thread, this might be related to "strong dominant bit" when multiple CAN transceivers source current on the bus at the same time.
However, I would still like to check if the voltage level of ACK bit shown below would have potential risk?
And is there any approach to lower down the voltage level of ACK bits?
Regards,
Charles