Part Number: TCA9539
Hi Team,
What is the recommended wiring of the exposed center pad?
Should it be connected to GND?
BR,
Stefan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9539
Hi Team,
What is the recommended wiring of the exposed center pad?
Should it be connected to GND?
BR,
Stefan
Hi Stefan,
There is nothing indicating in the datasheet that the "exposed center pad" is electrically connected to any of the external pins. This pad is for a more stable solder connection, but also serves as a thermal relief mechanism to pull heat away from the IC. Most will say to connect this center pad to GND due to the GND plane in most PCB's being a very large piece of metal which is good for thermal conduction. This exposed pad can either be connected to a GND plane or a VCC plane, whichever the customer prefers.
Main idea: connect the pad to a large piece of metal on the PCB.
Regards,
Tyler
The pad is glued to the substrate, which typically is at GND potential. The glue might be electrically conductive. So the pad, if not left floating, should not be connected to any other voltage than GND. See [FAQ] Where do I connect the thermal pad of the logic QFN devices?