Part Number: DS90UB960-Q1
Hi Team,
This is the continuation of the ticket "DS90UB960-Q1: Applying trigger on two camera sensor at the same time", Unfortunately i couldn't replay to that ticket.

Our requirement is whenever two trigger came at the same time in two image sensors , we should get both images without any miss.
Current Observation: images from two camera sensors are getting mixed up when applying trigger at the same time on both cameras.
Additional information:
-We are using external trigger to apply the trigger and currently there is no way of synchronization possible with this trigger signals.
-Currently Round Robin is being used as forwarding mode. [We are not able to capture the image once we changed the mode to any of the synchronized forwarding mode-( ie capture is getting completed-stuck, we suspect its due to the the precondition for synchronized forwarding is not met)]
-Only one csi port is being used to send the video data to the processor.
-We are using imx8mn processor, Virtual channel is not supported for imx8mn.[ Nxp Tech support team conformed]
-Is there any way we can get the images from both sensors as two frames if the trigger is happening at the same time?