This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6424A: Junction Temperature vs Ambient Temperature

Part Number: TCA6424A

The datasheet specifies "operating temperature" range "-40°C to +85°C".

The parameter name is "Ta" indicating that it refers to ambient temperature, right?

The abs max rating for storage is +150°C.

The thermal parameters all refers to junction temperature.

What is the recommended junction temperature range?

Is it 150°C or something in between 85°C and 150°C? (like 125°C)?

Best Regards

Bjorn