Part Number: DP83TC812EVM-MC
Other Parts Discussed in Thread: USB-2-MDIO
I have DP83TC812EVM-MC 2 Boards.
Already tested wake-up, sleep test case via user manual , Ther are working well.
(pull the wake pin high using the available jumper on the EVM, and send Reg 0x018c, 0002 wiring via USB-2-MDIO Tool)
But in this case, Master EVM was going to sleep
so, next wake-up I had to put the wake pin high
How can I do wake up, sleep of EVM remotely(by SW).
Wanted Test Case
1. Set Master , Set Slave
2. Master send Wake up message to Slave Board. (by SW)
3. Master send Sleep message to Slave Board. (In this time Master does not go to sleep mode, becuase I don't want to lost USB Connection )
4. Master send Wake up message to Slave Board again. (by SW)