Part Number: SN65DSI86EVM
Other Parts Discussed in Thread: SN65DSI86
Hello,
I am trying to use the SN65DSI86EVM MIPI to eDP bridge to connect my board on Debian Linux with the NXP i.MX8MP processor to a display with Display Port. I installed the necessary ti-sn65dsi86 driver as kernel module and wrote a device tree overlay. However the bridge doesn't seem to create any output. The dmesg show following regarding the bridge:
~# dmesg | grep dsi
[ 0.304040] i2c 1-002d: Fixing up cyclic dependency with 32e60000.mipi_dsi
[ 1.165697] ti_sn65dsi86 1-002d: GPIO lookup for consumer enable
[ 1.165713] ti_sn65dsi86 1-002d: using device tree for GPIO lookup
[ 1.165725] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/soc@0/bus@30800000/i2c@30a30000/sn65dsi86@2d[0]'
[ 1.165755] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/soc@0/bus@30800000/i2c@30a30000/sn65dsi86@2d[0]'
[ 1.165778] ti_sn65dsi86 1-002d: using lookup tables for GPIO lookup
[ 1.165783] ti_sn65dsi86 1-002d: No GPIO consumer enable found
[ 1.165790] ti_sn65dsi86 1-002d: Looking up vcca-supply from device tree
[ 1.165806] ti_sn65dsi86 1-002d: Looking up vcca-supply property in node /soc@0/bus@30800000/i2c@30a30000/sn65dsi86@2d failed
[ 1.165842] ti_sn65dsi86 1-002d: supply vcca not found, using dummy regulator
[ 1.166003] ti_sn65dsi86 1-002d: Looking up vcc-supply from device tree
[ 1.166017] ti_sn65dsi86 1-002d: Looking up vcc-supply property in node /soc@0/bus@30800000/i2c@30a30000/sn65dsi86@2d failed
[ 1.166044] ti_sn65dsi86 1-002d: supply vcc not found, using dummy regulator
[ 1.166088] ti_sn65dsi86 1-002d: Looking up vccio-supply from device tree
[ 1.166100] ti_sn65dsi86 1-002d: Looking up vccio-supply property in node /soc@0/bus@30800000/i2c@30a30000/sn65dsi86@2d failed
[ 1.166124] ti_sn65dsi86 1-002d: supply vccio not found, using dummy regulator
[ 1.166172] ti_sn65dsi86 1-002d: Looking up vpll-supply from device tree
[ 1.166184] ti_sn65dsi86 1-002d: Looking up vpll-supply property in node /soc@0/bus@30800000/i2c@30a30000/sn65dsi86@2d failed
[ 1.166207] ti_sn65dsi86 1-002d: supply vpll not found, using dummy regulator
[ 11.234765] auxiliary ti_sn65dsi86.bridge.0: deferred probe pending
Looks like the driver is looking for the necessary
- enable-gpios
- vccio-supply
- vpll-supply
- vcca-supply
- vcc-supply
But should they be specified in this case where we're using the Evaluation board?
The i2c address of the chip is being detected:
~# i2cdetect -y 1
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- 2d -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --
And when the dsi86-kernel module is inserted, the 0x2d address shows "UU".
I would appriciate any help on what I am doing wrong.