Part Number: DS100DF410
Hello,
I have the similar question about XFI to SFI interconnect and I found this thread.
Is it true that I can directly connect XFI to SFI from chip to chip to make them link up?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS100DF410
Hello,
I have the similar question about XFI to SFI interconnect and I found this thread.
Is it true that I can directly connect XFI to SFI from chip to chip to make them link up?
Hi,
Yes that's correct, you can use DS100DF410 to interconnect XFI and SFI interfaces.
Best,
Lucas
I see, DS100DF410 is a retimer to compensate PCB loss, not a protocol converter used to convert XFI to SFI.
If our PCB trace is short and PCB loss is very low, then SFI and XFI can interconnect directly. Is that true?
Hi Gang,
Data can be passed directly between XFI and SFI interfaces without any decoding or reencoding. XFI and SFI have different min/max electrical limits for high-speed electrical parameters, which means they can't necessarily be interconnected directly even with low insertion loss, although it may be possible. A retimer can be useful to improve signal integrity to meet the specs of both interfaces.
I suggest taking a look at the 10G XFI and SFI specifications.
INF-8077i_10G_xfp_xfi_spec.pdf
sff-8431_10G_sfp+_sfi_spec.pdf
Best,
Lucas