Part Number: DS250DF230
Hi,
First, let me explain my customer's situation.
<Customer's Situation>
The customer inputs signals at two different rates: 4.9152Gbps and 9.8304Gbps. In order to enable CDR locking of 4.9152Gbps and 9.8304Gbps signals, the customer has configured 4.9152Gbps and 9.8304Gbps data rate in manual mode.
So when the 9.8304Gbps signal is input, the 9.8304Gbps setting will be CDR Lock, but the 4.9152Gbps setting will be CDR not Lock. This is the behavior the customer expected.
But when the 4.9152Gbps signal is input, the 9.8304Gbps setting will be CDR Lock, but the 4.9152Gbps setting will be CDR Lock. The customer did not expect two types of signals to be CDR locked.
Therefore, the following operations are performed to determine which signal is being input.
・<When input 9.8304Gbps> Lock at 9.8304Gbps → Don't Lock at 4.9152Gbps → Lock at 9.8304Gbps → Determine 9.8304Gbps
・<When input 4.9152Gbps> Lock at 9.8304Gbps → Lock at 4.9152Gbps → Determine 9.8304Gbps
<My Question>
Is it possible to determine that 9.8304Gbps has been input by the following method?
*The figure below does not take into account the delay time.
Best Regards,
Nishie