Part Number: TIC12400-Q1
Hai Team,
We interfaced MSDI with microcontroller. The SPI Communication between switch and MCU is working. we are connected channel 0,2,4,6 as Ground connected. we are able to read the MSDI Device ID Register as well.
it returns as 0x20.
But we are unable to detect the Switch Change by reading the Status register(0x05) while pressing the switch. But it changes in the Hardware.
we wrote the attached configurations. Once the configuration is completed the voltage on the signal is increased to 4.5V( Why it is increasing). Actually it is 2.4V Without pressing the switch.
Please find the below configuration. Can you help me is there any configuration issue. The voltage before configuration is 2.4V with out pressing the switch and 1.3V with pressing the switch. we programmed 2V as comparator Threshold.
Step1:Enable input channels 0 2 4 6 (Requirement) Register 1BH 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 1 0 1 0 1 0 1 ---->0x000055 Setp2: Current Source Selection: Register 1CH Configure all to source selection [0h] 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ----> 0x000000 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 Step3: Wetting Current Configuration WC_CFG0 Register 1Dh : wetting current Configure to 2mA[2h] 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0x002092 0 0 0 0 0 0 0 0 0 0 1 0 0 0 0 0 1 0 0 1 0 0 1 0 WC_CFG1 Register 1EH : Wetting current configure to 2mA[2H] 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0X000000 0 0 0 0 0 0 0 0 0 0 1 0 0 0 0 0 1 0 0 1 0 0 1 0 Step4: Mode Selection Mode Register 32h 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0x000000 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 Step 5: Set Device Configuration Register Address 1AH Set trigger to 0 [Stop Device] VS Ratio to 1 - to support voltage range from 4.5 to 30v polling enabled INT_CONFIG - Interrupt Assertion to static crc disabled Polling activation time 1024us[bh] polling time 4ms [1h] 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0x953562 1 0 0 1 0 1 0 1 0 0 1 1 0 1 0 1 0 1 1 0 0 0 1 0 Step 6 : Comparator Thresholds Configuration THRES_COMP Register 21h: Set to 3h - threshold voltage to 2V Digital Inputs 00 02 04 06 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0x000000 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 Step 7 :Enable global interrupt on state change INT_EN_CFG0 Register 24h: Global Interput SSC_EN TO enable interrupt assertion on Switch State Change 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0x000004 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 1 0 0 Step 8: Interrupts detection configuration Register is 0x22 Digital Input 00,02,04,06 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0x003333 0 0 0 0 0 0 0 0 0 0 1 1 0 0 1 1 0 0 1 1 0 0 1 1 Step 9 : Enable Device to Start Operation: Now all the required settings done, enable trigger for normal operation CONFIG Register 1Ah: 23 22 21 20 19 18 17 16 15 14 13 12 11 10 9 8 7 6 5 4 3 2 1 0 ---> 0x812D62(Requirement) Step 9 : Monitor status IN_STAT_COMP IN_STAT_COMP Register 05h: Read the contetns of STAT_COMP Register to verify the changes but it is not changing with pressing the switch.