Part Number: DP83822IF
Hello,
I need to set LED_0 of DP83822IF to MII_LINK
and i need to set COL to operate as LINK_OK
When I looked at the datasheet, I understand that LED0 and COL pins are set in the MLEDCR register.
However, if I look at page 52 of the data sheet, it says “MLED can be routed to only noe of these two pins at a time.”
I understood that MLED settings were only possible with either LED0 or COL. Is that correct?
thank you