Part Number: DP83869HM
Other Parts Discussed in Thread: AM5748
Hello,
DP83869HM is interface to AM5748 through RGMII0 interface. Communication is established but link is not up. Since we are using RGMII to Copper mode, the GTX_CLK must be 125MHz but we are getting 2.5MHz. So Is this because of the GTX_CLK, link is not up or any other configuration is required. In hardware strapping PHY_ADD is set to 0XC and OPMODE[2:0]=000 which is RGMII to Copper Mode. What are the register configuration to be made to set into this mode?
Thanks,
Chaithra Kulal