Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869EVM
Hi team,
Using the MII interface of the STM32F407ZGT6 and the DP83869HM, the processor only supports 10/100M, so the initialization register configuration is as follows:
01DFH=0060H
0000H=3100H
0004H=01E1H
0009H=0000H
0010H=5048H
001FH=4000H
After the configuration is complete, the cycle reads some status register information as follows:
0001H=7949H
006EH=0400H
01DFH=0060H
0010H=5048H
0032H=00D0H
Plugging in and un-plugging the network cable does not reflect on the status register, what can be done to locate the cause of the problem?
The STM32F407ZGT6 and DP83848 have been used as MII and are working correctly.
The schematic is attached
Best Regards,
Amy