Part Number: DS90UB960-Q1
Hi,
Here is a description from Datasheet Page166.
"The VPOC noise must be kept to 10 mVp-p or lower on the source / deserializer side of the system. The VPOC fluctuations on the serializer side, caused by the sensor's transient current draw and the DC resistance of cables and PoC components, must be kept at minimum as well. Increasing the VPOC voltage and adding extra decoupling capacitance (> 10 µF) help reduce the amplitude and slew rate of the VPOC fluctuations."
When we talk about "noise", do we refer to the absolute Vpp of VPOC including the regulator output ripple and load transient and so on? What is the measure condition?
BTW, I read datasheets of other devices, and they define "VPOC" as the input voltage of regulator after POC on the serializer board. And Rin+ noise is required 10mVp-p max. Does DS90UB960-Q1 has the similar requirement?