Part Number: DS26LV31QML
Dear High Reliability team.
This part has 4 channel. but I use only 3 channel.
Should unused channels (input and output) be connected to GND or VCC?
Otherwise, Can I leave they OPEN?
thankyou
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS26LV31QML
Dear High Reliability team.
This part has 4 channel. but I use only 3 channel.
Should unused channels (input and output) be connected to GND or VCC?
Otherwise, Can I leave they OPEN?
thankyou
thank you for your answer.
I have an additional question.
What happens if unused input be left? the output of used channel occurs abnormal operating?
also, Can I place 10 Kohm pull-down resistor for unused input channel?
Letting an input float will increase power consumption, and might damage the device; see [FAQ] How does a slow or floating input affect a CMOS device?
The size of the input series resistor does not matter; it might as well be 0 Ω. You need 10 kΩ only if you want to change the level during debugging.