Part Number: TUSB9261
Hello, I am new in this topic ... I have System-On-Module board without SATA interface but with several USB3.0. I hope is it possible to use this chip here right? I want to connect typical M.2 Key-B+M SSD drive with SATA interface to my SOM as a typical storage device like pendrive but with a lot of space. I downloaded Burner application and firmware with U1/U2 disabled but I need it in Limux Mint version. In another topic I saw that I have to ask You TI for linux version. Am I correct? And the last question ... what do You think is the best option to use USB_VBUS pin in that kind of storage devices? Short it to 3V3 with resistor divider?


As You see I have only 3V3 and maybe some other voltages generated for specific IC's like 1V8 for some GPIO's from SMARC 2.0 and 1V1 for TUSB9261. In that module I have some USB modules but that I need to use don't have VBUS_DET, only other pin is EN_OC#. This is bidirectional pin for something like here (power switch with overcurrent fault#). So I think the best option is to connect with divider +3V3_SSD to USB_VBUS in TUSB9261. What do You think?