Part Number: DP83867IR
Hi Team,
This post is related to the following.
The default value of RGMIICTL[1:0] differs depending on the sample.
Sample A: Register 0x0032, RGMIICTL is 0x00D3
Sample B: Register 0x0032, RGMIICTL is 0x00D0
The read value of Register 0x006E and 0x006F after pin-RESET is same in two system .
Register 0x006E is 0x0000
Register 0x006F is 0x0100
Is it possible that the default value differs depending on the lot?
Best Regards,