This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TC812EVM-MC: MDIO

Part Number: DP83TC812EVM-MC

I have Questions.

First

end sleep command to DP83TC812EVM-MC via USB2MDIO SW,  It's working. (Reg Adress: 0x018c, Data: 0002)

When I sent the command to  DP83TC812EVM-MC via Arduino Interface of MDIO,  It was not working, 

Standard Reg Address's format of MDIO is 5 bits. so different bit size between Stand format and USB2MDIO.

Which data have to be sent?, if I want to send sleep mode(TC10) ?

Second.

Is it limited Speed of MDIO commnunication ?

When I sent MDC/MDIO data from external mcu(Arduino) to EVB , It was wrong response from EVB (MDC of Arduino is 500Hz )

Thanks.