Part Number: DS34RT5110
Other Parts Discussed in Thread: SN65DP159, SN65DP149, , TMDS181, TDP0604, TDP1204, TMDS1204
Hi Team,
When connected through LAN cable, the communication is failed and the display of screen is not normal if the length of cable exceeds 2 meters. So please check an attachment and recommend the redriver or retimer solution. The EDID, CEC, HPD signals of HDMI source are not connected to the redriver or retimer, the only TMDS signals are connected to it. And the customer is considering to design the configuration of method 2.
Regards,