Other Parts Discussed in Thread: LMH1228, , USB2ANY
Hello
I designed a 4k-SDI dual 1 to 4 distributor using LMH1219 as equalizer and LMH1228 as driver as you see in the block diagram.

This is my EQ and DR schematic


In my design I have to use back panel and so I don't have on board BNC connectors.
This is my back panel's picture

You can see my EQ circuit on PCB

And DR circuit:

I tried to have space between EQs and DRs and power section

Also on the back panel I draw a good GND plane between equalizers and drivers

With all this considerations When I enabled all drivers to have output, I can not get more than 25m with Belden-1694 on equalizers while datasheet says it can work with 75m. when I turn off drivers, equalizers will lock more than 60m(I can see on Lock LED). I don't know why drivers effect on equalizer signal and what should I do to prevent this problem. Do you have any advice?
If there is a good simulation tools that I can use to understand where is the problem, please introduce me.
Thanks.