Part Number: TUSB2E22
Hi,
We would like to have further information on the parametric measurement setup for the repeater. Please check below for the snapshot from the TUSB2E22 datasheet.

1) We need further description about the test channel.
2) Impedance conversion formula.
We also checked the Eval Board Schematic (check below)

eUSB
3) R5, R9 are 0ohm here and R6, R8 has been highlighted as DNI. Can we conclude that R6 and R8 resistors are required only for repeater eye diagram measurements where R5 and R9 need to be 22ohms?
4) For our on-board designs we can follow the EVB schematic with the 0ohm resistors for R5 and R9 and there will be no impedance mismatch issues.
USB2.0
5) There is no provision on the USB2.0 side on the EVB to populate 143ohm shunt resistors to GND and 15.8ohm series resistors for the Test Channel as per the parametric measurement information block diagram. So do we need to take care of the impedance matching for our designs on the USB2.0 side?
Please clarify.
Thanks,
Venkat