Other Parts Discussed in Thread: SK-AM62B-P1, SK-AM62B
Hi,
I'm hoping this inconsistency can be cleared up. I would like to bring your attention to the following forum question from more than 5 years ago below...
In this forum question it was recommended NOT to use the LINK-PP LPJG16314A4NL RJ-45 due to the center taps being connected together. We are doing a new design with the AM623x (AM6232) and the DP83867IRRGZT (PHY). We have purchased the AM62x EVK's (SK-AM62B and SK-AM62B-P1) which use the combination of the AM62x, DP83867 and Link PP LPJG16314A4NL RJ-45 w/Integrated magnetics. Can I get an explanation why this NOT recommended RJ-45 connector is being used 5 years later on recently released EVK's?
Regards,
Davey