This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125MB203: Interface forum:When the HDMI signal passes through the DS125MB203 equalizer, the signal quality is reduced, find out why

Part Number: DS125MB203
Other Parts Discussed in Thread: TMDS181, TDP0604, TS3DV642, HD3SS215

The HDMI signal goes through the DS125MB203 equalizer and the signal quality goes down. Don't know where the equalizer is set up to go wrong?
I packed the customer's schematics and some of the waveforms from the test into a file to get you to check them out.

Add:1. The faster the speed, the worse the eye image; the eye image of HDMI 2.0 is significantly worse than HDMI1.4. 

        2.The HDMI connector is connected to the DS125MB203 via AC (The HDMI connector is connected to the DS125MB203 via AC).

Thank you very much!

 

Best Regards,

Arabella Zhang

 

weixinnuo.zip