Other Parts Discussed in Thread: DS90CF383B, , SN65LVDS93B-Q1
Hi, TI expert
The customer was using DS90CF383MTD, but was looking for a replacement due to discontinuation.
So, DS90CF383B was recommended, but the operating temperature was -10 to 70 degrees, which did not meet the spec. (The specification of the customer’s product is -40 to 85 degrees.)
Accordingly, the two items that the customer directly searched for were SN65LVDS93AIDGGRQ1 and SN65LVDS93BIDGGRQ1. (Actually used P-CLK is 50~70MHz.)
The customer purchased samples of SN65LVDS93AIDGGRQ1 and SN65LVDS93BIDGGRQ1 and conducted a test.
However, upon review, a malfunction was confirmed as described in the attached review.
Q1) Can you provide technical help to solve the problem? (See attached file below)
Q2) Will there be any problem if I use SN65LVDS93A-Q1 or SN65LVDS93B-Q1 as a replacement for DS90CF383MTD?
Please check. Thank you.