Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041: The USB2.0 is disconnected occasionally

Part Number: TUSB8041

When the CPU started,it can’t connect the USB HUB( TUSB8041) occasionally.

 

Restart the TUSB8041, sometimes it will work well, and sometimes the USB 2.0 will disconnect.

 

When the USB 2.0 disconnected, the CPU UART0 will print like this:

 

Compare above, when the USB 2.0 connected, the CPU UART0 will print like this:

 The SCH is below:

 8041.pdf