Part Number: DS15BA101
Other Parts Discussed in Thread: DP83869HM, , SN65LVDS100
Hello There,
we use DP83869HM as PHY for 100M media converter. In order to connect Optical receiver we need to meet PHY input specification of 0.3-2.0 V for differential signals (8.5 datasheet).
Our Receiver has differential output of 0.19 - 0.32 V which not fully in spec of PHY.
We need simple reliable device allowing interface between receiver and PHY, with minimum form factor, low price, minimum additional components.
We chose your DS15BA101 as buffer. RX (0.19-0.39V) --> DS15BA101 (0.4V) --> DP83869HM (0.3-2.0V)
We would like to ask:
- Is this fully compatible?
- Is there another buffer more suitable for this application?
- Should it be always RX --> DS15 --> DP83639 AC coupled at all interfaces for proper functionality
Usually in most other device datasheets (SN65LVDS100) is differential voltage level 250-450 mV - Does this mean, it is not compatible with the PHY? or this voltage level is double?
Initial topic was started already in PHY forum: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1342757/dp83869hm-pair-of-phys-falling-out-of-sync/5123129#5123129
Thank you for help here.
Best
Michael