Part Number: DS90UB948-Q1
Dear team,
Q1: Do we need falling edge to detect INT signal Low?
Q2: If Q1 is yes and INTB remains low after power up. Doesn't this IC detect INTB low?
Thank you.
Yuto Kitamura
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB948-Q1
Dear team,
Q1: Do we need falling edge to detect INT signal Low?
Q2: If Q1 is yes and INTB remains low after power up. Doesn't this IC detect INTB low?
Thank you.
Yuto Kitamura
Hi Logan,
Thank you, please provide the answer once you get any updates.
Yuto Kitamura
Yuta-san,
I tested this, RX_REM_INT is always asserted on start-up anyways as a transient, so it will always have the host controller initially try to service downstream device, regardless of whether it was initially held low on device PDB.
Also, as mentioned before, INTB is falling edge detection, so after the initial interrupt clear on start-up/PDB release - interrupt will not re-assert until next falling edge.
Regards,
Logan