Part Number: TCAN1145-Q1
Other Parts Discussed in Thread: ESD2CAN24
Hi, Support Team
schematic as below chart: have any concern?

Q1: About TCAN1145A
- How to placement termination resistors? Follow EVB termination resistors near transceiver IC or datasheets chapter 13 “Layout” (near connector)?
- About SPI. Is only nINT/SDO need external pull-up 10k ohm (inner open drain)? Other pins can use internal pull-up resistors(~350 k ohm)? (Datasheet Figure 10-5. ;REVISED MARCH 2022)
- About INH pin, need external pull-down 100k ohm for inner PMOS open drain.
Q2: about WAKE pin
- I only can image, a mechanical if can provide voltage transition will trigger that device wake-up, right?
- The “WAKE” detection “H”(“L”) to “L”(“H”) (VHmin = Vsup-2V, VLmax = Vsup-3.5V) divider from Vsup.
- How to design “WAKE” pins parallel capacitor? Datasheet is 22nF. But EVM is 0.01uF. Which is better
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence