Part Number: TMDS1204
Hi Team,
I am using TMDS1204 in my design. I2C communication is not responding. Also HPD_IN connection following same as application circuit given in datasheet. I.e. HPD_IN is connected to connector with pull up of 5V (hdmi connector not on board 5V). If I connect loopback cable then I2C starts responding. So below are my queries
1. Is there any relation between HPD_IN and I2C bus to be active?
2. In sink application, HPD_signa is output from SoC. So What is exact HPD_IN and HPD_OUT connection if I use TMDS1204 as sink application? I believe HPD_IN should drive by SoC and HPD_OUT should connect to HDMI RX connector.
Also attached my circuit diagram for your reviewTMDS1204_schematics.pdf
Thanks,
Venkatesh