Part Number: DS125DF1610EVM
Other Parts Discussed in Thread: USB2ANY
I installed the snlc055e (SigCon Architect EVM GUI setup with RTE) on my windows 10 PC. Turned on the 2.5V power supply, connect the USB to the PC (also tried to connect USB first then turn on 2.5V), then open the SigCon Architect GUI, I always get the same message "There are no USB2ANY interface detected". I also tried to tie J193 pin 1-2 and pin 3-4 (the board came with them open), still no luck. So I wonder what else can be wrong. Do I need to update the MSP430 firmware? How to do that? The EVM kit came with a SPA dongle, but the user guide did not talk about how to use the dongle.
Also there is one weird thing happened on this board. The 3.3V power supply is shot with ground (verified this with multimeter). I wonder why? Did I get a bad board? I can only use 2.5V power supply.
Thanks,
Wendy