Part Number: SN65DSI85
Hi Team
I have a problem with the SN65DSI85-Q1, I can't lock on the mipi clk. The value of the mipi clk is around 150MHz, I can measure the frequency with the scope, but I can't get pll locked. The bit 0 in the E5 register is always 1, after I write FF into the register. The equalization (register 0x11) doesn't help. I used a dsi tuner and read a datasheet to create an initialization sequence.
The mipi clk can be used even to read a test pattern, but I can't use it to read an actual input data.
I can get a data in the FPGA when I use a REFCLK X 2 (I use an evaluation board, 27MHz X 2 = 54MHz), but in this case lvds clk slightly higher than actual pixel clk, which is around 150MHz/3 = 50MHz. I wanted to understand what happening in this case: do I get some padding (like blank pixels) or something else? Can I work in this mode? What will be effect on the picture?
Regards
Dany