Part Number: MAX3227
I am using the MAX3227 chip and I have it interfaced as such,
On boot, V+ and V- are 2.5 V instead of 5.5V. Ready pin is low and Invalid pin is low. (It doesn't go to 5.5 V at all on boot, which makes me think it is going directly into shutdown).
On the Rin, I have a test probe connected to an external device with a -5V signal (stable as the device I am connected to only responds when given a command). On the Din, I have a TTL signal coming from an FPGA that is sending the command. I have checked the Din and it is sending the TTL command signal.
I have tested all of my equipment on a breadboard and it was working fine the only difference was that I had the FORCEON driven high to force normal operation.
The AutoShutdown seems to not be working as I have a valid Rin signal and I should be getting edge detection on the Din side. I am unsure what I am doing wrong on my side.