Part Number: TUSB9261
Other Parts Discussed in Thread: TUSB9260
Tool/software:
Hello,
As per previous communication I include USB to SATA converter circuitary in my main board.
I refered reference schematic of TUSB9261 and accordingly I include those sections in my design. Now My board is assembled it has TUSB9261 and my CPU. They were communicating through USB 3.0 interface.
My CPU had Linux Ubuntu OS.
There is only one difference I made while assembling the board. As per schematic W25x512 flash memory suppose to be put but I had SST25vf080B (8Mb) flash memory so I put that.
I had download SLL416 firmware. In that different firmware files are there. I had select TUSB926x_FW_v1.06.bin firmware.(I had doubt of which format should be loaded .bin or .hex?)
I had CH341a flash programmer through that I flashed memory.
When I power on the board and scaned USB peripherals then in that list TUSB9261 is detected as vendor specific device.
In later stage I connect SATA SSD drive to my board but unfortunately its not get detect.
I checked supplies and clock frequencies. I am getting 1.1V,3,3V supplies properly. Also crystal output also come exactly 40MHz. I connect serial port of chip to debug port but there I am not getting any debug (basically baud rate is not known).
Device is detected by CPU but drive is not get detected.
I checked 1:1 and cross SATA connection but drive is not getting detected.
Please guide me on how to check my circuitary?
Thanks.