Other Parts Discussed in Thread: TFP410
Hi,
I am designing a board with a TFP410 connected to an FPGA.
The output of the TFP410 is connected to a Samsung 961E monitor.
The image is 1024*768 pixels.
The clock freq. (IDCK+) is 50MHz.
Hsync and Vsync are active high for 256 clpcks , during which time DE is low.
Hsync, Vsync and DE change together on the rising edge of the clock.
The TFADJ resistor is 510 Ohm and connected to 3v3.
PD pin is connected to 3v3 ->Power UP
ISEL is low. ->I2C disabled
EDGE is high ->Rising Edge
BSEL is high -> 24 Bit
DKEN is low ->DSKEW disabled
CTL1 CTL2 CTL3 are low.
All the inputs to the TFP410 were sampled with a scope and appear to be OK.
The TFP410 outputs appear to be active and the clock is clean.
Our monitor remains black, so it seems that we are still missing some definition.
The TFP410 data sheet does not have much information concerning timing and does not describe any special requirements needed to initialize the monitor
Do you have any suggestions?
Thanks for your help.
Lior
lglick@iai.co.il