Part Number: SN65HVD1786
Other Parts Discussed in Thread: SN65HVD1787,
Tool/software:
Hi Parker,
Sorry for the delay of the answer. Are those SN65HVD1786 or SN65HVD1787 models ? (because the names of the libraries are "1786").
Thank you !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD1786
Other Parts Discussed in Thread: SN65HVD1787,
Tool/software:
Hi Parker,
Sorry for the delay of the answer. Are those SN65HVD1786 or SN65HVD1787 models ? (because the names of the libraries are "1786").
Thank you !
Hi Louca,
So - really sorry about that confusion.
SN65HVD1787_typicalSpecModel.lib
I seemed to have made the model for the 1786 not the 1787 - that being said I was able to create the correct 1787 model (biggest thing is drive speed difference which is just a very simple parameter change).
The same caveats apply for the model.
The RX_path model I sent in the last thread would be the same for the 1787 so you can use that as a stand-in as from a modeling perspective they are the same.
I apologize for that confusion once again!
Best,
Parker Dodson