Part Number: TCAN4550
Tool/software:
Hello,
while the standard bit rates configurations works well, when I configure low data bit rates the communication fails.
for example, when arbitration bit rate is 50kb/s and data bit rate is 500kbit/s the communication works well without errors.
but when arbitration bit rate is 50kb/s and data bit rate is 100kbit/s (DBTP = 0x180C11 , DBRP = 25 TSEG1 = 13 ,TSEG2 = 2 , SJW = 1 ) the communication fails.
the bus is populated with two bus nodes, both use the above part.
any suggestions?