Part Number: TPD6E004
Tool/software:
Hello Team,
This post is a continuation of one of my previous post link
As per the application note slva680a, the ESD /TVS diode must be connected to the chassis ground.
In our system, these diodes are connected to the system ground only.
1). Is there any problem with this?.
2). Which is the best way to connect the ESD diode?
3). Also, can I directly connect the chassis Ground to the Earth Ground?.
4). In our design, the shield of the USB, RJ45 are connected to the chassis ground directly and these shields are connected to the singal ground through resistor parallel to capacitor in multiple places.
Will this create any ground loop in the system?.
5). Can you please review the ground diagram below.?
Looking for your reply